ACTION#.TASKID

Description

Some tasks require a task ID to specify what is acted upon. For example, if setting the value of DOUT2 from the source, then ACTION#.TASK = 1 (set Digital Output from Source), and ACTION#.TASKID = 2.

ACTION#.TASK must be set before ACTION#.TASKID. If ACTION#.TASK is modified, then the range and units of ACTION#.TASKID may be modified, and the value will be defaulted.

Not all tasks require a task ID.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

Depends on ACTION#.TASK

Default Value

Depends on ACTION#.TASK

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

ACTION1.TASKID

3908h

01h

Unsigned8

-

-

Read/Write

No

ACTION2.TASKID

3908h

02h

Unsigned8

-

-

Read/Write

No

ACTION3.TASKID

3908h

03h

Unsigned8

-

-

Read/Write

No

ACTION4.TASKID

3908h

04h

Unsigned8

-

-

Read/Write

No

ACTION5.TASKID

3908h

05h

Unsigned8

-

-

Read/Write

No

ACTION6.TASKID

3908h

06h

Unsigned8

-

-

Read/Write

No

ACTION7.TASKID

3908h

07h

Unsigned8

-

-

Read/Write

No

ACTION8.TASKID

3908h

08h

Unsigned8

-

-

Read/Write

No

ACTION9.TASKID

3908h

09h

Unsigned8

-

-

Read/Write

No

ACTION10.TASKID

3908h

0ah

Unsigned8

-

-

Read/Write

No

ACTION11.TASKID

3908h

0bh

Unsigned8

-

-

Read/Write

No

ACTION12.TASKID

3908h

0ch

Unsigned8

-

-

Read/Write

No

ACTION13.TASKID

3908h

0dh

Unsigned8

-

-

Read/Write

No

ACTION14.TASKID

3908h

0eh

Unsigned8

-

-

Read/Write

No

ACTION15.TASKID

3908h

0fh

Unsigned8

-

-

Read/Write

No

ACTION16.TASKID

3908h

10h

Unsigned8

-

-

Read/Write

No

ACTION17.TASKID

3908h

11h

Unsigned8

-

-

Read/Write

No

ACTION18.TASKID

3908h

12h

Unsigned8

-

-

Read/Write

No

ACTION19.TASKID

3908h

13h

Unsigned8

-

-

Read/Write

No

ACTION20.TASKID

3908h

14h

Unsigned8

-

-

Read/Write

No

ACTION21.TASKID

3908h

15h

Unsigned8

-

-

Read/Write

No

ACTION22.TASKID

3908h

16h

Unsigned8

-

-

Read/Write

No

ACTION23.TASKID

3908h

17h

Unsigned8

-

-

Read/Write

No

ACTION24.TASKID

3908h

18h

Unsigned8

-

-

Read/Write

No

ACTION25.TASKID

3908h

19h

Unsigned8

-

-

Read/Write

No

ACTION26.TASKID

3908h

1ah

Unsigned8

-

-

Read/Write

No

ACTION27.TASKID

3908h

1bh

Unsigned8

-

-

Read/Write

No

ACTION28.TASKID

3908h

1ch

Unsigned8

-

-

Read/Write

No

ACTION29.TASKID

3908h

1dh

Unsigned8

-

-

Read/Write

No

ACTION30.TASKID

3908h

1eh

Unsigned8

-

-

Read/Write

No

ACTION31.TASKID

3908h

1fh

Unsigned8

-

-

Read/Write

No

ACTION32.TASKID

3908h

20h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

ACTION1.TASKID

40900

9FC4

Unsigned8

Read/Write

-

ACTION2.TASKID

40901

9FC5

Unsigned8

Read/Write

-

ACTION3.TASKID

40902

9FC6

Unsigned8

Read/Write

-

ACTION4.TASKID

40903

9FC7

Unsigned8

Read/Write

-

ACTION5.TASKID

40904

9FC8

Unsigned8

Read/Write

-

ACTION6.TASKID

40905

9FC9

Unsigned8

Read/Write

-

ACTION7.TASKID

40906

9FCA

Unsigned8

Read/Write

-

ACTION8.TASKID

40907

9FCB

Unsigned8

Read/Write

-

ACTION9.TASKID

40908

9FCC

Unsigned8

Read/Write

-

ACTION10.TASKID

40909

9FCD

Unsigned8

Read/Write

-

ACTION11.TASKID

40910

9FCE

Unsigned8

Read/Write

-

ACTION12.TASKID

40911

9FCF

Unsigned8

Read/Write

-

ACTION13.TASKID

40912

9FD0

Unsigned8

Read/Write

-

ACTION14.TASKID

40913

9FD1

Unsigned8

Read/Write

-

ACTION15.TASKID

40914

9FD2

Unsigned8

Read/Write

-

ACTION16.TASKID

40915

9FD3

Unsigned8

Read/Write

-

ACTION17.TASKID

40916

9FD4

Unsigned8

Read/Write

-

ACTION18.TASKID

40917

9FD5

Unsigned8

Read/Write

-

ACTION19.TASKID

40918

9FD6

Unsigned8

Read/Write

-

ACTION20.TASKID

40919

9FD7

Unsigned8

Read/Write

-

ACTION21.TASKID

40920

9FD8

Unsigned8

Read/Write

-

ACTION22.TASKID

40921

9FD9

Unsigned8

Read/Write

-

ACTION23.TASKID

40922

9FDA

Unsigned8

Read/Write

-

ACTION24.TASKID

40923

9FDB

Unsigned8

Read/Write

-

ACTION25.TASKID

40924

9FDC

Unsigned8

Read/Write

-

ACTION26.TASKID

40925

9FDD

Unsigned8

Read/Write

-

ACTION27.TASKID

40926

9FDE

Unsigned8

Read/Write

-

ACTION28.TASKID

40927

9FDF

Unsigned8

Read/Write

-

ACTION29.TASKID

40928

9FE0

Unsigned8

Read/Write

-

ACTION30.TASKID

40929

9FE1

Unsigned8

Read/Write

-

ACTION31.TASKID

40930

9FE2

Unsigned8

Read/Write

-

ACTION32.TASKID

40931

9FE3

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.TASKID

40900

Unsigned8

Read/Write

-

ACTION2.TASKID

40901

Unsigned8

Read/Write

-

ACTION3.TASKID

40902

Unsigned8

Read/Write

-

ACTION4.TASKID

40903

Unsigned8

Read/Write

-

ACTION5.TASKID

40904

Unsigned8

Read/Write

-

ACTION6.TASKID

40905

Unsigned8

Read/Write

-

ACTION7.TASKID

40906

Unsigned8

Read/Write

-

ACTION8.TASKID

40907

Unsigned8

Read/Write

-

ACTION9.TASKID

40908

Unsigned8

Read/Write

-

ACTION10.TASKID

40909

Unsigned8

Read/Write

-

ACTION11.TASKID

40910

Unsigned8

Read/Write

-

ACTION12.TASKID

40911

Unsigned8

Read/Write

-

ACTION13.TASKID

40912

Unsigned8

Read/Write

-

ACTION14.TASKID

40913

Unsigned8

Read/Write

-

ACTION15.TASKID

40914

Unsigned8

Read/Write

-

ACTION16.TASKID

40915

Unsigned8

Read/Write

-

ACTION17.TASKID

40916

Unsigned8

Read/Write

-

ACTION18.TASKID

40917

Unsigned8

Read/Write

-

ACTION19.TASKID

40918

Unsigned8

Read/Write

-

ACTION20.TASKID

40919

Unsigned8

Read/Write

-

ACTION21.TASKID

40920

Unsigned8

Read/Write

-

ACTION22.TASKID

40921

Unsigned8

Read/Write

-

ACTION23.TASKID

40922

Unsigned8

Read/Write

-

ACTION24.TASKID

40923

Unsigned8

Read/Write

-

ACTION25.TASKID

40924

Unsigned8

Read/Write

-

ACTION26.TASKID

40925

Unsigned8

Read/Write

-

ACTION27.TASKID

40926

Unsigned8

Read/Write

-

ACTION28.TASKID

40927

Unsigned8

Read/Write

-

ACTION29.TASKID

40928

Unsigned8

Read/Write

-

ACTION30.TASKID

40929

Unsigned8

Read/Write

-

ACTION31.TASKID

40930

Unsigned8

Read/Write

-

ACTION32.TASKID

40931

Unsigned8

Read/Write

-